Solution
Wave Energy Converter
Wave energy converters, or WEC’s, devices that convert the mechanical energy of waves into electrical energy.
Custom submersible ISHK-B Bow Type Crosby™ Cabled Load Shackles
SGA AC/DC Powered Signal Conditioner
Customer control center
Interface’s custom made submersible ISHK-B Bow Type Crosby™ Cabled Load Shackles are attached to the mooring lines, which is connected to the wave energy converter. An electric cable is connected which can then start creating power.
The SGA AC/DC Powered Signal Conditioner can connect to the customers control center, where force tension data can be remote monitored.